About the Momentary push button's error state
The error state shows at runtime if:
- The Value connection is unassigned
- The Indicator connection value does not match one of the configured state values
Provide Feedback