Set up connections for a Macro button
The
Macro
button runs a specified macro when the operator presses it at runtime.To set up tags and expressions for the Macro button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign tags and expressions to the connections for the macro name, as necessary.TIP:The macro name must be a string type.
Provide Feedback