Set up general properties for a local message display

Use the
General
tab of the
Local Message Display Properties
dialog box to set up general options for a local message display.
To set up general options for a local message display
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
TIP:
Use
|n
for a new line in your messages in the message file to control where a message begins a new line. Or you can select the
Word wrap
option to let the application begin a new line when the next word will not fit on the current line.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal