Set up connections for a local message display
Use the
Connections
tab of the Local Message Display Properties
dialog box to set up connections for a local message display.To set up connections for a local message display
- In theGraphics Displayeditor, double-click the display to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign tags or expressions to the connections:
- Value
- Message File, if you want to use a variable message file
- Echo Message, if you want to write the triggered message to a tag
Provide Feedback