Set up states for a Latched push button

Use the
States
tab of the
Latched Push Button Properties
dialog box to set up states for the button.
To set up states for a Latched push button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    States
    tab.
  3. In the
    Select state
    list, click
    State 0
    .
  4. Specify these properties for State 0:
    • Value
    • General appearance
    • Caption, if any
    • Image, if any
  5. Repeat steps 3 and 4 for State 1 and the Error state.
Once you set up the general, caption, and image properties for one state, copy and paste the state’s properties to another state or to all states.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal