Set up general properties for a Latched push button
Use the
General
tab of the Latched Push Button Properties
dialog box to set up how the button looks.To set up general options for a Latched push button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Once you set up the options on the
General
tab, click the States
tab to specify how the object looks in each state at runtime.Provide Feedback