Set up connections for a Goto Display button
When selected at runtime, the
Goto Display
button opens the graphic display assigned to the button. To set up tags and expressions for a Goto Display button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to the Display Name, Top Position, and Left Position connections, as necessary.TIP:The Display Name must be a string type. The Top Position and Left Position connections must be numeric types. Valid values must be an integer between ‑32768 to 32767.
Provide Feedback