How the Goto Display button works at runtime

When the operator presses the
Goto Display
button at runtime, the graphic display assigned to the button opens.
The
Goto Display
button’s behavior at runtime also depends on which types of graphic displays are already open and which type of display it is opening.
Use display types
  • If the graphic display assigned to the button is a Replace display, it closes any open On Top or Replace displays. It does
    not
    close any On Top displays that use the
    Cannot Be Replaced
    option.
  • If the graphic display assigned to the button is an On Top display (with or without the
    Cannot Be Replaced
    option) and you select the
    Display position enabled
    option (on the
    General
    tab), the display is positioned using the "Top position" and "Left position" settings. Otherwise, the display is positioned using the graphic display’s settings.
  • The operator cannot use this button to open Replace displays if display change is currently controlled remotely. But the operator can still open On Top displays (with or without the
    Cannot Be Replaced
    option).
    TIP:
    The types of displays and the graphic display's settings are configured in the
    Display Settings
    editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal