Causes of runtime errors for a Goto Display button

At runtime, the assigned graphic display does not open, and the application logs errors to diagnostics about the
Goto Display
button if:
  • The display assigned to the button has been deleted from the project.
  • The operator does not have security access for the display.
  • The display assigned to the button is the display that contains the button.
  • The display change is controlled remotely (by the data source) and a Replace display is assigned to the button.
  • The parameter file assigned to the button has been deleted from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal