Set up general properties for a Goto Display button

Use the
General
tab of
Goto Display button Properties
dialog box to set up how a
Goto Display
button looks.
To set up general options for a Goto Display button
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
Once you set up the options on the
General
tab, click the
Label
tab to specify a caption or image for the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal