Set up values and thresholds for a gauge
Use the
Display
tab to set up values and thresholds for a gauge.To set up values and thresholds for a gauge
- In theGraphics Displayeditor, double-click the gauge to open itsPropertiesdialog box.
- Click theDisplaytab.
- Specify these properties:
- Minimum and maximum values
- Legends, if any
- Thresholds, if any
Provide Feedback