Set up connections for a gauge
Use the
Connections
tab of the Gauge Properties
dialog box to set up a tag or expression for the object.To set up tags and expressions for a gauge
- In theGraphics Displayeditor, double-click the gauge to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to this connection:ValueA read connection. You can assign a tag or an expression to this connection. The application reads the value of the connection at the data source and updates the object’s display to reflect the value.If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the value.
Provide Feedback