Set up general properties for a gauge
Use the
General
tab of the Gauge Properties
dialog box to set up how a gauge looks.To set up general options for a gauge
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Once you set up the options on the
General
tab, click the Display
tab to specify the values and thresholds for the object.Provide Feedback