Causes of runtime errors for a Display Print button

At runtime, the application logs errors about the
Display Print
button to diagnostics under these circumstances:
Printer occupied
If the printer is currently printing when the operator presses the
Display Print
button, the display is not printed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal