Set up handshaking for a control list selector
When the operator presses the
Enter
key, the application writes a value to the data source. Use Enter key handshaking to hold the value at the data source for a specific period of time to ensure it is read before the operator sends a new value to the Value connection.To set up handshaking for a control list selector’s buttons
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theTimingtab.
- Specify the handshaking settings to use with theEnterkey.
Provide Feedback