Set up connections for a control list selector
Use the
Connections
tab of the Control List Selector Properties
dialog box to set up tags and expressions for the object.To set up tags and expressions for a control list selector
- In theGraphics Displayeditor, double-click the selector to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to these connections:ValueAssign a tag to this connection. When the operator selects a state, the application writes the value corresponding to the selected state to the tag’s data source. The application also monitors this connection and if the value changes, highlights the new state in the list.The Value connection triggers the state's action. For example, when the tag assigned to the connection changes to a new state, the data source changes a motor's speed to a new setting.TIP:IfWrite on enteris selected on theGeneraltab, the application does not write to the Value connection until the operator selects a state and pressesEnter.IfWrite on enteris not selected on theGeneraltab, the application writes to the Value connection as soon as a state is selected. The Enter and Enter Handshake connections are ignored.EnterThis connection accepts values of 0 and 1 only. The connection determines how long theEnterkey press is registered. Use this connection for Enter key handshaking.Enter HandshakeYou can assign a tag or an expression to this connection. This connection resets the Enter connection, using the Handshake reset type property specified on theTimingtab. Use this connection for Enter key handshaking if you want the Enter connection to be reset when a value at the data source changes.If you assign an expression, the application calculates the value of the expression and resets the Enter connection when the expression value meets the conditions of the Handshake reset type option.
Provide Feedback