Set up states for a control list selector
Use the
States
tab to set up how the control list selector's appearance changes to match the value of the Indicator connection.To set up states for a control list selector
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theStatestab.
- From theSelect statelist, selectState 0.
- Specify these properties for State 0:
- Value
- Caption, if any
- Repeat steps 3 and 4 for each additional state.
Once you set up the properties for one state, you can copy and paste the state’s properties to another state or to all states.
TIP:
To add or remove a state without returning to the
General
tab, click Insert State
or Delete State
.Provide Feedback