Hold a value for a specified length of time

One method of using Enter key handshaking is to hold the value at the data source for a specified period of time. For this method, assign a tag to the Enter connection and specify the
Enter
key hold time.
Enter
key control delay is optional.
To set up Enter key handshaking to hold the value at the Value connection for a certain length of time
  1. In the
    Timing
    tab, specify a time for the
    Enter
    key hold time, and, optionally, the
    Enter
    key control delay.
  2. In the
    Connections
    tab, assign a tag to the Enter connection. A digital tag is recommended.
How this type of handshaking works
  • When the user presses the
    Enter
    key, the value is sent to the Value connection.
  • If there is a time specified for the
    Ente
    r key control delay, the delay timer begins timing. When the time is up, the Enter connection is set to 1. If no time is specified for the
    Enter
    key control delay, the Enter connection is set to 1 as soon as the user presses the
    Enter
    key.
    As long as the Enter connection is set to 1, the user cannot send new values to the Value connection.
  • When the Enter connection is set to 1, the
    Enter
    key hold time timer begins timing. When the time expires, the Enter connection is reset to 0 and new values can be sent to the Value connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal