Causes of runtime errors for a control list selector

At runtime, the application logs errors about the control list selector to diagnostics under these circumstances:
Value connection unassigned
If the Value connection is unassigned:
  • Nothing is written to the Value connection.
  • The cursor remains on the unselected state.
  • The highlight bar does not appear.
  • The application logs an error.
Invalid values
If a state’s value is too large for the data type of the tag assigned to the Value connection, or if the value is outside the assigned tag’s minimum and maximum values:
  • The application does not write the value to the Value connection.
  • The highlight remains as is.
  • The application logs an error.
For example, the state value is too large for the tag’s data type if your data source is a
PLC-5®
, the state value is 2,147,483,647, and the assigned tag is an integer tag using the address N7:0. Integer tags have a range of -32,768 to 32,767 only.
If Enter key handshaking is set up and
Write on enter
is selected on the
General
tab, the Enter connection is not set to 1, and the handshake timers do not begin timing.
Enter key handshaking in effect
If the control list selector’s Enter key handshaking is still in effect when the operator presses the
Enter
button:
  • Nothing is written to the Value connection.
  • The cursor remains on the unselected state and the highlight remains on the selected state.
  • The Enter connection remains set to 1 and the handshake timers continue timing.
  • The application logs an error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal