Set up connections for a Close Display button

Use the
Connections
tab to set up a tag or expression for the
Close Display
button.
To set up a tag or expression for a Close Display button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag to this write connection. Assign a tag that can receive the integer value specified in the
    Close value
    box on the
    General
    tab.
    Value
    When the operator presses the
    Close Display
    button, the application writes the integer value specified in the Close value property to the tag’s data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal