How the Close Display button works at runtime

When the operator presses the button at runtime, the graphic display that the button is on closes. If the
Write on Close
check box on the
General
tab is checked, when the button is pressed, the value specified in the
Close
value box (
General
tab) is written out to the location specified in the
Connections
tab.
If the graphic display that is closing is a Replace display, and display change is controlled remotely (by the data source), the display does not close.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal