Causes of runtime errors for a Close Display button

At runtime, the display does not close and the application logs errors about the
Close Display
button to diagnostics if:
  • The
    Close Display
    button is on a Replace display, and display change is controlled remotely (by the data source).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal