Set up general properties for a Clear Audit Trail button

Use the
General
tab of the
Properties
dialog box to specify how the
Clear Audit Trail
button looks.
To set up general properties for a Clear Audit Trail button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify these properties:
    • General appearance
    • Touch margins
    • Audio (whether the button beeps at runtime)
Once you set up the options on the
General
tab, click the
Label
tab to set up a caption and image for the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal