Set up connections for a bar graph
Use the
Connections
tab of the Bar Graph Properties
dialog box to set up a tag or expression for the object.To set up tags and expressions for a bar graph
- In theGraphics Displayeditor, double-click the bar graph to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to this connection:ValueA read connection. You can assign a tag or an expression to this connection. The application reads the value of the connection at the data source and changes the fill level on the bar graph to reflect the value.If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the value.
Provide Feedback