Set up general properties for a bar graph

Use the
General
tab of the
Bar Graph Properties
dialog box to set up how a bar graph looks.
To set up general options for a bar graph
  1. In the
    Graphics Display
    editor, double-click the object to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal