Test animation
To test the animation you have set up on a graphic display, use
Test Display
to switch to test mode. When you finish testing, switch back to edit mode to continue editing.To switch between test and edit modes, do one of the following:
- From theViewmenu, selectTest DisplayorEdit Display
- On the toolbar, click
or
.
TIP:Test mode is not the same as running the display. Test mode does not change the appearance or position of the display as set up in theDisplay Settingsdialog box. Also, data logging is not turned on in test mode.
Provide Feedback