Set up hyperlink animation

To set up hyperlink animation for an object
  1. Select the object.
  2. From the
    Animation
    menu, select
    Hyperlink
    .
  3. On the
    Hyperlink
    tab, in the
    Address
    box, specify an expression that represents the linked destination by any of the following methods:
    • Type a URL address or a file path. It must be enclosed in double quotes (“ ”). When entering a URL address on a
      PanelView Plus 7
      or
      PanelView Plus 6
      terminal, you must include the protocol name, such as
      http://
      and
      https://
      .
    • Click
      Tag
      to browse for a string tag that represents the URL address or a file path.
    • Click
      Expression
      to open the
      Expression Editor
      to create one.
    • Click
      Browse for File
      to browse and select a file.
    • Click
      Browse the Web
      to open the default browser on your computer. Then browse to the web page you want to link to, and copy and paste the URL to the
      Expression
      box.
  4. When finished, click
    Apply
    .
    TIP:
    If an object’s hyperlink animation address is a path to a nonexistent file, clicking this object on a
    PanelView Plus 7
    or
    PanelView Plus 6
    terminal will launch the file type associated program or show an error message.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal