Copy and paste animation

You can copy the animation defined for one graphic object in a display and then paste it onto another object. Use
Copy Animation
and
Paste Animation
options on the
Edit
menu to do this.
To copy the animation from an object
  1. Select the object whose animation is to be copied.
  2. Choose
    Copy Animation
    from the
    Edit
    menu.
To paste the animation to another object
  1. Select the objects to which the animation is to be copied.
  2. From the
    Edit
    menu, select
    Paste Animation
    .
    TIP:
    You can select the object, then open the relevant
    Animation
    dialog box to review the details of the animation before you copy it. You do not have to close the
    Animation
    dialog box to copy the animation. From the
    Edit
    menu., select
    Copy Animation
    .
    When you paste animation onto an object, it overrides and merges with any existing animation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal