Close the Object Explorer
You can close the
Object Explorer
in multiple ways.To close the Object Explorer, do one of the following
- From theViewmenu, selectObject Explorer.
- Click theClosebutton on the top right hand corner of theObject Explorer.
- On the graphic display, right-click to open the context menu and then selectObject Explorer.
Provide Feedback