Web Browser ActiveX control

The Web Browser ActiveX control provides the system with the ability to show web pages from an HMI application.
IMPORTANT:
You can run the Web Browser ActiveX control only on a
MobileView
terminal, a
PanelView Plus 7 Performance
terminal, or a
PanelView Plus 6
terminal with extended features, as Web Browser ActiveX control uses
Internet Explorer
, which is only available for a
MobileView
terminal, a
PanelView Plus 7
Performance terminal, or a
PanelView Plus 6
terminal with extended features.
On a
PanelView Plus 7 Performance
Series B terminal, the Web Browser ActiveX control becomes a button, which opens the specified URL in
Microsoft
Edge
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal