ResetPassword ActiveX control

The ResetPassword ActiveX control allows any user to modify any other user's password in the system. The intent of the control is to allow someone in an administrative role to reset a user's password.
Use the ResetPassword ActiveX control to:
  • Specify a target user account name
  • Specify new and confirmation passwords
  • Report results of password reset operation
The ResetPassword ActiveX control is only available on
MobileView
,
PanelView Plus 7
, and
PanelView Plus 6
terminals.
TIP:
  • The ResetPassword ActiveX control does not validate the current user's rights to modify another user's password. When applying the ResetPassword ActiveX control, only give access to the authorized users for security.
  • The ResetPassword ActiveX control should be applied in a pop-up display that uses user security to restrict access.
  • The HMI Designer must provide String Entry objects for the operator to specify user account name, password, and confirmation password.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal