Program Launcher ActiveX control
The Program Launcher ActiveX control provides the system with the ability to launch
third-party applications from within the
FactoryTalk View ME
application.Use the Program Launcher ActiveX control to:
- Launch a specified instance of an application with optional command parameters
- Control focus of launched application(s), bringing the desired application to the foreground under application control
- Close specific applications launched using the control
TIP:
To ensure consistency when launching
Microsoft®
Edge™
using ME Program Launcher, we recommend that you turn
off Startup Boost
and Continue running background extensions and apps when
Edge is closed
in Edge
, and set the LaunchEnable and
NewInstance parameters to 1 in FactoryTalk View Studio
. For more information, see
Knowledgebase Document ID: QA78619 - FactoryTalk View Studio Machine Edition: ME
Program Launcher Launches Microsoft Edge Inconsistently.Provide Feedback