Display ActiveX control

The Display ActiveX control provides the system with the ability to open and close OnTop and Replace displays. When a display is opened, a parameter file can be specified.
Use the Display ActiveX control to:
  • Open an OnTop or a Replace display
  • Specify a parameter file to be passed to the display during opening
  • Close an OnTop or Replace display
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal