Edit messages
Use the
String Edit
dialog box to edit existing messages and to insert embedded variables in messages. You can use embedded variables in local messages, information messages, and alarm messages.To edit messages
- From theEditmenu, selectEdit String, or right-click theMessagecolumn and selectEdit String.
- Type the message text in the text box.
- (Optional) ClickInsert variable.
- From the list, select the type of variable to be inserted in the caption.
- In the dialog box, specify the details of the variable.TIP:Embedded variables are case sensitive, and must be in the proper format and syntax to work. If you make a mistake, your variable will be treated as a piece of text. Therefore, do not attempt to edit embedded variables manually. Use theInsert VariableandEdit variabledialog boxes to avoid problems.
Provide Feedback