Create local messages
Use the
Local Messages
editor to create local messages and specify their trigger values. You can define up to 10,000 messages in each message file.To create local messages
- In theGraphicsfolder in theExplorerwindow, double-click theLocal Messagesicon to open the editor.
- Specify the messages and their trigger values.
- From theFilemenu, selectSaveand specify a name for the file.
- ClickClose.TIP:If you rename any of your local message files, make sure you update any local objects that use that message file to the new name.TheDelete Row(s)menu item on theEditmenu does not delete multiple selected rows in certain spreadsheet editors. If you select multiple rows in theInformation Messages,Local Messages,Macros,and Alarm Setup (Messages tab)editors, and then selectDelete Row(s)from theEditmenu, only one row will be deleted.To delete multiple rows, right-click in the editor and selectDelete Row(s).
Provide Feedback