Set up information messages
Follow the steps below to set up information messages.
To set up information messages
- In theInformation Messageseditor, set up the messages and their trigger values.
- In theInformation Setupeditor:
- Specify the graphic display to open when information messages occur, and the file of messages to show.
- Assign a tag or expression to theValueconnection.If you want the operator to acknowledge messages, assign theAckconnection and specify the acknowledge hold time.
- In theStartupeditor, select theInformation messagescheckbox is selected.
- (Optional) In theGraphicseditor, modify the default [INFORMATION] display or create your own graphic display to use for information messages.For example, if you don’t want the operator to acknowledge messages, edit the default display to remove the information acknowledge button.TIP:When renaming information message files, update the reference to the message file in theInformation Setupeditor to the new name.
Provide Feedback