Set up how information messages are shown

Use the
Information Setup
editor to set up how information messages are shown.
Select the
Information messages
check box in the
Startup
editor to turn on information messages at runtime.
TIP:
  • If you use the Information Acknowledge button, configure the data source to change the Value connection to 0 when the Ack connection changes to 1. Then acknowledging the message closes the information display.
  • When renaming information message files, make sure you update the reference to the message file in the Information Setup editor to the new name.
To set up how information messages are shown
  1. Double-click the
    Information Setup
    icon to open the editor.
  2. Specify these options:
    • The graphic display to use for information messages
    • The file of messages to show
    • The acknowledge hold time, if any
  3. Assign a tag or expression to these controls:
    • Value
    • Ack
  4. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal