Where you can create embedded variables

You can create embedded variables in these editors:
  • Graphics
    . Use this editor to insert embedded variables in the captions for graphic objects or in any text objects. For graphic objects with multiple states, you can insert different embedded variables in each state’s caption.
  • Local Messages.
    Use this editor to insert embedded variables in local messages.
  • Information Messages.
    Use this editor to insert embedded variables in information messages.
  • Alarm Setup
    . Use this editor to insert embedded variables in alarm messages.
  • Display Settings.
    Use this editor to insert embedded variables in the title bars of displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal