Embed a variable in a text object
You can insert embedded variables in any graphic text objects. At runtime, the text will be updated with the real-time values of the variable.
To insert an embedded variable in a text object
- Double-click the text object you want to set up.
- Click theGeneraltab containing the text box.
- In the text box, type the text as desired.
- At the point where you want to embed the variable, clickInsert Variable.
- Select the type of variable you want to insert.
- Define the variable and clickOK.
Provide Feedback