Embed a variable in a message
You can embed variables in local messages, information messages and alarm messages. Create the message as you normally would, and at the point where you want to insert a variable, open the
Edit String
dialog box.To open a dialog box for creating an embedded variable in a message
- In theLocal Messages,Information Messages, orAlarm Setupeditor, right-click in theMessagecolumn and then clickEdit String.orFrom theEditmenu, selectEdit String.
- ClickInsert Variable.
- Select the type of variable to insert.
- Specify the options.
Provide Feedback