Open a recently used application
You can open a recently used application from the
File
menu.To open a recently used application
- From theFilemenu, selectRecent Applications.
- Click the application name in the list.
- If an application is already open,FactoryTalk View Studioasks you whether to close the application. ClickYes.
The application opens in the language that it was last opened.
Provide Feedback