Change Application Language dialog box

How do I open the Change Application Language dialog box?
In
FactoryTalk View Studio
, from the
Application
menu, select
Change Application Language
, or click the
Change Application Language
icon on the toolbar.
Use the
Change Application Language
dialog box to switch application languages at design time.
The text in the following dialog boxes will be changed to the selected language:
  • Alarm Setup
  • Display
  • Global objects
  • Information Messages
  • Local Messages
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal