Excel spreadsheet checking orders during import
When importing an Excel spreadsheet to an application, the import operation checks the Excel spreadsheet in the following order:
- Language columns whose language does not exist in the application
- Component types that are invalid
- Server names that do not exist in the application
- Component names that do not exist in the application
- Descriptions that do not exist in the application
- Duplicate string references pointing to strings that do not exist in the spreadsheet
Provide Feedback