Go to Configuration Mode on a terminal when an application is running

You can go to Configuration Mode on a terminal when an application is running.
To go to Configuration Mode on a terminal when an application is running
  • Put a
    Goto Configure Mode
    button on a display. Open the display and press the button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal