Set up global Macro connections
Use the
Macro
tab of the Global Connections
editor to set up global Micro connections.To set up global Macro connections
- On theMacrotab, in theMaximum update rate (seconds)box, select the maximum rate at which the data source will supply data to the global connections.
- (optional) Define up to five expressions or tags, each of which can run a corresponding macro.
TIP:
To unassign a control, select the control in the
Tag
or Expression
column and do one of the following:- PressBackspaceon your keyboard repeatedly to remove the assignment one character at a time.
- Double-click twice to highlight the text, and then pressDeleteorBackspaceto remove the entire assignment at once.
Provide Feedback