Causes of runtime errors for global connections

At runtime, the application logs errors about global connections to diagnostics if:
  • The Display Number or Remote Display Number control contains a non-existent display number.
  • The time or date received from the data source is invalid.
  • The data source triggers a display print but the printer is not responding.
  • The data source triggers a display print but the runtime system does not have enough memory to capture the display image.
  • Any of the expressions assigned to the connections are invalid or contain invalid assignment statements.
  • An expression has been defined to run a macro, and the macro does not exist.
The application logs a warning if the operator attempts to change graphic displays when display changes are controlled remotely by the data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal