Name the project

Use this dialog box to name the project.
To name the project
  • In the text box, type a name for the new HMI project to be created from the backed up file, and then click
    Finish
    .
If the name is the same as an existing project, an error message will show. If the name is valid, the operation will proceed.
When you enter a new application name, do not exceed 32 characters. If the application name exceeds the maximum 32 characters allowed by
FactoryTalk View Studio
, errors and warning messages will show.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal