Delete an application
Use this dialog box to delete an application.
TIP:
When deleting an application, you will not be prompted to validate user rights.
When deleting a project, the project's unique security configuration will also be deleted.
To delete an application
- SelectDelete applicationand clickNext.
- From the list, select the application you want to delete, and then clickNext.
- For Machine Edition applications, the HMI server project referenced by the ME application is deleted together.
- ClickFinish. ClickYesto confirm the deletion.
Provide Feedback