HMI server properties (General tab)

The
General
tab of the
HMI Server Properties
dialog box displays information about the HMI server and lets you change its description.
To modify the general properties
  1. In the
    Explorer
    window, right-click the HMI server icon and then select
    Properties
    from the
    Context
    menu.
  2. In the
    General
    tab add or change the description.
  3. Click
    Apply
    to save the changes.
Options
  • Name
    Displays the name of the HMI server. You cannot change it.
  • Description
    You can add text to describe the HMI server or edit an existing description.
  • Project file
    Shows the location of the HMI server project file.
  • Number of displays
    Shows the number of displays contained in the HMI server project.
  • Licensed maximum
    Shows the maximum number of displays that can be contained in the HMI server project. The activation key that the HMI server is using sets this limit.
    TIP:
    Adding faceplate displays to an application affects the license count. Each added faceplate display (.gfx file) counts as one display for activation purposes. The corresponding global object display (.ggfx file) does not add to the total license count.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal