What is a recipe file?
A recipe file is a specific set of data values that are associated with a specific set of tags. The function of the recipe system is to allow a runtime operator to write each data value to its associated tag in one operation.
A recipe file consists of:
- A runtime recipe name
- A status tag
- A percent-complete tag
- One or more ingredients
- One or more data sets
- One or more tag sets
- One or more recipe units
Provide Feedback